R_TAUm_Channeln_Get_PulseWidth

Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin.

[Syntax]

#include r_cg_macrodriver.h

void R_TAUm_Channeln_Get_PulseWidth ( uint32_t * const width );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

I/O

Argument

Description

O

Unit32_t * const width;

Pointer to an area to store the measurement width (0x0 to 0x1FFFF)

[Return value]

None.