R_TAUm_Channeln_Higher8bits_Start

Starts the count (higher 8-bit) for channel n.

Remark This API function can only be called when the timer array unit is used as an 8-bit timer.

[Syntax]

void R_TAUm_Channeln_Higher8bits_Start ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.