r_taum_channeln_higher8bits_interrupt

Performs processing in response to the timer interrupt INTTMmnH.

Remark This API function is called as the interrupt process corresponding to the timer interrupt INTTMmnH.

[Syntax]

CA78K0R Compiler

__interrupt static void r_taum_channeln_higher8bits_interrupt ( void );

CC-RL Compiler

static void _near r_taum_channeln_higher8bits_interrupt ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.