R_TAUm_Set_PowerOff

Halts the clock supplied to the timer array unit.

Remark Calling this API function changes the timer array unit to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void R_TAUm_Set_PowerOff ( void );

Remark m is the unit number.

[Argument(s)]

None.

[Return value]

None.