Usage example (Interval timer)

Enter the interrupt function at fixed intervals and count the number of interrupt occurrence.

[Waveform example]

[GUI setting example]

Timer

Used

TAU0

Used

Channel0

Channel 0

Interval timer

Intervalvalue (16 bits)

100μs (Actual value:100)

Generates INTTM00 when counting is started

Unused

End of timer channel0 count, generate an interrupt (INTTM00)

Used

Priority (INTTM00)

Low

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start TAU0 channel 0 counter */

R_TAU0_Channel0_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}

r_cg_timer_user.c

/* Start user code for global. Do not edit comment generated here */

volatile uint8_t g_cnt = 0U;

/* End user code. Do not edit comment generated here */

static void __near r_tau0_channel0_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

/* Count INTTM00 */

g_cnt++;

/* End user code. Do not edit comment generated here */

}