Usage example (Square wave output)

Perform toggle operation at fixed intervals and output a suquare wave with a duty factor of 50%.

[Waveform example]

[GUI setting example]

Timer

Used

TAU0

Used

Channel0

channel 0

Square wave output

Square width

100μs (Actual value:100)

Generates INTTM00 and inverts timer output when counting is started

Unused

Initial output value

0

End of timer channel0 count, generate an interrupt (INTTM00)

Used

Priority (INTTM00)

Low

[API setting example]

r_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start TAU0 channel 0 counter */

R_TAU0_Channel0_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}