debugger.Performance.Set


This function sets performance measurement. [RH850][E1/E2/E20/Full-spec emulator]

[Specification format]

debugger.Performance.Set(PerformanceCondition)

[Argument(s)]

Argument

Description

PerformanceCondition

Specify a condition of performance measurement.

See the PerformanceCondition class for a condition of performance measurement.

[Return value]

If performance measurement was set successfully: Performance measurement event number

If there was an error when setting performance measurement: None

[Detailed description]

-

This function sets performance measurement according to the contents specified with PerformanceCondition.

[Example of use]

>>>pf = PerformanceCondition()
>>>pf.StartAddress = 0x1000
>>>pf.EndAddress = 0xffe000
>>>pf.EndData = 0x10
>>>pf.EndPerformanceType = PerformanceType.Read
>>>pf.PerformanceMode = PerformanceMode.MaxCount
>>>pf.PerformanceItem = PerformanceItem.AllFetchBranch
>>>ps = debugger.Performance.Set(pf)
1
>>>print ps
1
>>>