debugger.Ie.GetValue

debugger.Ie.SetValue


This function sets or refers to the IE register or DCU register.

[Specification format]

debugger.Ie.GetValue(ieType, address)
debugger.Ie.SetValue(ieType, address, value)

[Argument(s)]

Argument

Description

ieType

Specify a register.

The registers that can be specified are shown below.

Type

Description

IeType.Reg

IE register [[IECUBE] 78K0] [[IECUBE] RL78] [[IECUBE] 78K0R] [[IECUBE] V850] [[IECUBE2] V850] [[Full-spec emulator] RH850]

IeType.Dcu

DCU register [[IECUBE] V850] [[IECUBE2] V850] [[Full-spec emulator/E1/E20] RH850]

address

Specify the address to reference/set.

value

Specify the setting value.

[Return value]

debugger.Ie.GetValue is the register value (numeric value)

debugger.Ie.SetValue is True if the setting was completed successfully, or False if there was an error when setting the register.

[Detailed description]

-

debugger.Ie.GetValue displays the value of the register specified by address.
The register type is specified by ieType.

-

debugger.Ie.SetValue writes value to the register specified by address.
The register type is specified by ieType.

Remark

When the DCU register is referenced, the register value is reset to 0.

[Example of use]

>>>debugger.Ie.GetValue(IeType.Reg, 0x100)
0x12
>>>debugger.Ie.SetValue(IeType.Reg, 0x100, 0x10)
True
>>>debugger.Ie.GetValue(IeType.Reg, 0x100)
0x10
>>>