debugger.Disconnect


This function disconnects from the debug tool.

[Specification format]

debugger.Disconnect()

[Argument(s)]

None

[Return value]

If the debug tool was disconnected successfully: True

If there was an error when disconnecting from the debug tool: False

[Detailed description]

-

This function disconnects from the debug tool.

[Example of use]

>>>debugger.Disconnect()
True
>>>