debugger.Trace.Information


This function displays conditional trace information.

[Specification format]

debugger.Trace.Information()

[Argument(s)]

None

[Return value]

List of conditional trace information (see the TraceEventInfo class for detail)

[Detailed description]

-

This function displays conditional trace information is shown by the following format.

trace-event-number Trace state start-address - end-address

[Example of use]

>>>ti = debugger.Trace.Information()
1 Trace Enable main - sub
>>>print ti[0].Number
1
>>>print ti[0].Name
Trace
>>>