debugger.ActionEvent.Enable


This function enables an action event setting.

[Specification format]

debugger.ActionEvent.Enable(actionEventNumber = "")

[Argument(s)]

Argument

Description

actionEventNumber

Specify the action event number to enable.

[Return value]

If an action event setting was enabled successfully: True

If there was an error when enabling an action event setting: False

[Detailed description]

-

This function enables the action event specified by actionEventNumber.

-

If actionEventNumber is not specified, then events of all action event numbers will be enabled.

[Example of use]

>>>debugger.ActionEvent.Enable(1)
True
>>>debugger.ActionEvent.Enable()
True
>>>