debugger.Whereami


This function displays a location.

[Specification format]

debugger.Whereami(address)

[Argument(s)]

Argument

Description

address

Specify the address of the location to display.

[Return value]

Strings of the location

[Detailed description]

-

This function displays the location at the address specified by address.

-

The location is normally displayed in the following format.

file-name#function-name at file-name#line-number

 

However, if the function or line number at that address is not found, then the location is displayed in the following format.

at symbol-name+offset-value

 

If the symbol is not found, then the location is displayed in the following format.

at address-value

 

If address is omitted, then the location of the pc value is displayed.

[Example of use]

>>>debugger.Whereami()
foo.c#func at foo.c#100
>>>debugger.Whereami(0x100)
foo.c#main at foo.c#20
>>>