Comparator B (CMPB)
Below is a list of API functions output by the Code Generator for Comparator B use.
Table 3.33 API Functions: [Comparator B]
API Function Name |
Function |
Performs initialization necessary to control the Comparator B. | |
Performs user-defined initialization relating to the Comparator B. | |
Performs processing in response to the comparator B interrupt. | |
Starts comparison for analog input voltage. | |
Ends comparison for analog input voltage. |