Data operation circuit (DOC)
Below is a list of API functions output by the Code Generator for data operation circuit.
Table 3.34 API Functions: [Data Operation Circuit]
|
API Function Name |
Function |
|
Performs initialization necessary to control the data operation circuit. | |
|
Performs user-defined initialization relating to the data operation circuit. | |
|
Performs processing in response to the data operation circuit interrupt. | |
|
Sets the operating mode and the initial value of the reference value for use by the data operation circuit. | |
|
Sets the input value (value for comparison with, addition to, or subtraction from the reference value) for use by the data operation circuit. | |
|
Gets the result of operation. | |
|
Clears the data operation circuit flag. |