LCD controller / driver (LCD)
Below is a list of API functions output by the Code Generator for LCD controller / driver use.
Table 3.37 API Functions: [LCD controller / driver]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the LCD controller / driver.  | |
| 
       Performs user-defined initialization relating to the LCD controller / driver.  | |
| 
       Sets the LCD controller / driver to display on status.  | |
| 
       Sets the LCD controller / driver to display off status.  | |
| 
       Enables operation of internal voltage boost circuit and capacitor split circuit.  | |
| 
       Disables operation of internal voltage boost circuit and capacitor split circuit.  |