Everything

Comparator C (CMPC)

Below is a list of API functions output by the Code Generator for Comparator C use.

 

Table 3.36 API Functions: [Comparator C]

API Function Name

Function

R_CMPC_Create

Performs initialization necessary to control the Comparator C.

R_CMPC_Create_UserInit

Performs user-defined initialization relating to the Comparator C.

r_cmpc_cmpcn_interrupt

Performs processing in response to the comparator C interrupt.

R_CMPCn_Start

Starts comparison for analog input voltage.

R_CMPCn_Stop

Ends comparison for analog input voltage.