Independent watchdog timer (IWDT)
Below is a list of API functions output by the Code Generator for independent watchdog timer use.
Table 3.24 API Functions: [Independent Watchdog Timer]
API Function Name |
Function |
Performs initialization necessary to control the independent watchdog timer. | |
Performs user-defined initialization relating to the independent watchdog timer. | |
Performs processing in response to the non-maskable interrupt (WUNI). | |
Performs processing in response to the non-maskable/maskable interrupt. | |
Clears the independent watchdog timer counter and resumes counting. |