Interrupt controller (ICU)
Below is a list of API functions output by the Code Generator for interrupt controller use.
Table 3.6 API Functions: [Interrupt Controller]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the interrupt controller.  | |
| 
       Performs user-defined initialization relating to the interrupt controller.  | |
| 
       Performs processing in response to the external pin interrupts.  | |
| 
       Performs processing in response to the software interrupt.  | |
| 
       Performs processing in response to the software interrupt2.  | |
| 
       Performs processing in response to the NMI pin interrupt.  | |
| 
       Allows detection of the external pin interrupt.  | |
| 
       Prohibits detection of the external pin interrupt.  | |
| 
       Allows detection of the software interrupt.  | |
| 
       Allows detection of the software interrupt2.  | |
| 
       Prohibits detection of the software interrupt.  | |
| 
       Prohibits detection of the software interrupt2.  | |
| 
       Generates the software interrupt.  | |
| 
       Generates the software interrupt2.  |