>>>info = debugger.XTrace.Dump(10)
853 00h00min00s001ms704us000ns 0x000002c2 movhi 0xffff, gp, r1
854 00h00min00s001ms706us000ns 0x000002c6 id.w 0x7ff4[r1], r6
855 00h00min00s001ms706us000ns 0x03ff9000 R 0x00000000
856 00h00min00s001ms706us000ns 0x000002ca movhi 0xffff, gp, r1
857 00h00min00s001ms710us000ns 0x000002ce movea 0x7ff8, r1, r7
858 00h00min00s001ms712us000ns 0x000002d2 jarl _main+0x36
859 00h00min00s001ms716us000ns 0x000002dc br _main+0x36
860 00h00min00s001ms720us000ns 0x00000312 prepare lp, 0x4
861 00h00min00s001ms720us000ns 0x03ff9308 W 0x000002d6
862 00h00min00s001ms724us000ns 0x00000316 br _main+0x2
>>>print info[0].FrameNumber
853
>>>print info[0].Timestamp
1704000
>>>print info[0].FetchAddress
706
>>>print info[0].Mnemonic
movhi 0xffff, gp, r1
>>>print info[0].ReadAddress
None
>>>print info[0].ReadData
None
>>>print info[0].IsDma
False
>>>
>>>print info[2].FrameNumber
855
>>> print info[2].Timestamp
1706000
>>>print info[2].FetchAddress
None
>>>print info[2].Mnemonic
None
>>>print info[2].ReadAddress
67080192
|