3.2.7 Buses

Below is a list of API functions output by the Code Generator for buses use.

Table 3.7

API Functions: [Buses]

API Function Name

Function

R_BSC_Create

Performs initialization necessary to control the buses.

R_BSC_Create_UserInit

Performs user-defined initialization relating to the buses.

r_bsc_buserr_interrupt

Performs processing in response to the bus error (illegal address access).

R_BSC_Error_Monitoring_Start

Allows the detection of bus errors (illegal address access).

R_BSC_Error_Monitoring_Stop

Prohibits the detection of bus errors (illegal address access).

R_BSC_InitializeSDRAM

Performs initialization of SDRAM controller.