Renesas Electronics
Below is a list of API functions output by the Code Generator for event link controller use.
Table 3.10
API Functions: [Event Link Controller]
API Function Name
Function
R_ELC_Create
Performs initialization necessary to control the event link controller.
R_ELC_Create_UserInit
Performs user-defined initialization relating to the event link controller.
r_elc_elsrni_interrupt
Performs processing in response to the event link interrupt.
R_ELC_Start
Starts interlinked operation of peripheral functions.
R_ELC_Stop
Ends interlinked operation of peripheral functions.
R_ELC_GenerateSoftwareEvent
Generates the software event.
R_ELC_Set_PortBuffern
Sets the value of a port buffer.
R_ELC_Get_PortBuffern
Gets the value of a port buffer.