Renesas Electronics
Below is a list of API functions output by the Code Generator for Comparator B use.
Table 3.33
API Functions: [Comparator B]
API Function Name
Function
R_CMPB_Create
Performs initialization necessary to control the Comparator B.
R_CMPB_Create_UserInit
Performs user-defined initialization relating to the Comparator B.
r_cmpb_cmpbn_interrupt
Performs processing in response to the comparator B interrupt.
R_CMPBn_Start
Starts comparison for analog input voltage.
R_CMPBn_Stop
Ends comparison for analog input voltage.