3.2.31 D/A converter (DA)

Below is a list of API functions output by the Code Generator for D/A converter use.

Table 3.31

API Functions: [D/A Converter]

API Function Name

Function

R_DA_Create

Performs initialization necessary to control the D/A converter.

R_DA_Create_UserInit

Performs user-defined initialization relating to the D/A converter.

R_DAm_Start

Starts D/A conversion.

R_DAm_Stop

Ends D/A conversion.

R_DAm_Set_ConversionValue

Sets the data for D/A conversion.