Renesas Electronics
Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 3 use.
Table 3.13
API Functions: [Multi-Function Timer Pulse Unit 3]
API Function Name
Function
R_MTU3_Create
Performs initialization necessary to control the multi-function timer pulse unit 3.
R_MTU3_Create_UserInit
Performs user-defined initialization relating to the multi-function timer pulse unit 3.
r_mtu3_tgimn_interrupt
Performs processing in response to the input capture/compare match interrupt.
r_mtu3_tcivn_interrupt
Performs processing in response to the overflow interrupt.
r_mtu3_tciun_interrupt
Performs processing in response to the underflow interrupt.
R_MTU3_Cn_Start
Starts counting by a 16-bit timer.
R_MTU3_Cn_Stop
Ends counting by a 16-bit timer.