3.2.15
Port output enable 3 (POE3)
Below is a list of API functions output by the Code Generator for port output enable 3 use.
Table 3.15 | API Functions: [Port Output Enable 3] |
|
|
|
|
R_POE3_Create
|
Performs initialization necessary to control the port output enable 3.
|
|
R_POE3_Create_UserInit
|
Performs user-defined initialization relating to the port output enable 3.
|
|
r_poe3_oein_interrupt
|
Performs processing in response to the output enable interrupt n (OEIn).
|
|
R_POE3_Start
|
Places the MTU's complementary PWM output pins in the high-impedance state.
|
|
R_POE3_Stop
|
Releases the R_POE3_Stop MTU's complementary PWM output pins from the high-impedance state.
|