Renesas Electronics
Below is a list of API functions output by the Code Generator for compare match timer W use.
Table 3.21
API Functions: [Compare Match Timer W]
API Function Name
Function
R_CMTWn_Create
Performs initialization necessary to control the compare match timer W.
R_CMTWn_Create_UserInit
Performs user-defined initialization relating to the compare match timer W.
r_cmtw_cmwin_interrupt
Performs processing in response to the compare match interrupt.
r_cmtw_icmin_interrupt
Performs processing in response to the input capture interrupt.
r_cmtw_ocmin_interrupt
Performs processing in response to the output compare interrupt.
R_CMTWn_Start
Starts counting by a 16-bit timer.
R_CMTWn_Stop
Ends counting by a 16-bit timer.