Description
Below is a list of output file files by the Code Generator.
Table 2.1 Output File List (1/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_main.c or r_cg_main.c | A A | ||
| r_systeminit.c or r_cg_sysmteminit.c | A A | ||
| r_cg_macrodriver.h | - | - | |
| r_cg_userdefine.h | - | - | |
| r_cg_cgc.c | A M A A A A A A | ||
| r_cg_cgc_user.c | M A A A A | ||
| r_cg_cgc.h | - | - | |
| r_cg_port.c | A | ||
| r_cg_port_user.c | M | ||
| r_cg_port.h | - | - | |
| r_cg_hofc.c | A A A | ||
| r_cg_hofc_user.c | M A | ||
| r_cg_hofc.h | - | - | |
| r_cg_timer.c or r_cg_tau.c | R_TAUm_Channeln_Higher8bits_Start R_TAUm_Channeln_Lower8bits_Start R_TAUm_Channeln_Higher8bits_Stop R_TAUm_Channeln_Lower8bits_Stop | A A A A A A A M A A A | |
| r_cg_timer_user.c or r_cg_tau_user.c | M A A | ||
| r_cg_timer.h or r_cg_tau.h | - | - | 
Table 2.2 Output File List (2/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_timer.c or r_cg_tmrj.c | A A A A A A A A M M | ||
| r_cg_timer_user.c or r_cg_tmrj_user.c | M A M A | ||
| r_cg_timer.h or r_cg_tmrj.h | - | - | |
| r_cg_timer.c or r_cg_tmrd.c | A A A M M M A M M M A A A A M | ||
| r_cg_timer_user.c or r_cg_tmrd_user.c | M A M A | ||
| r_cg_timer.h or r_cg_tmrd.h | - | - | |
| r_cg_timer.c | A A A M A | ||
| r_cg_timer_user.c | M A | ||
| r_cg_timer.h | - | - | 
Table 2.3 Output File List (3/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_tmrx.c | A A A A M | ||
| r_cg_tmrx_user.c | M A | ||
| r_cg_tmrx.h | - | - | |
| r_cg_timer.c or r_cg_tmkb.c | R_TMR_KBm_BatchOverwriteRequestOn R_TMR_KBm_ForcedOutput_mn_Start | A A A M A A A A A M | |
| r_cg_timer_user.c or r_cg_tmkb_user.c | M A | ||
| r_cg_timer.h or r_cg_tmkb.h | - | - | |
| r_cg_timer.c | A A A M | ||
| r_cg_timer_user.c | M A | ||
| r_cg_timer.h | - | - | |
| r_cg_kb2.c | R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Start R_KB2m_TKBOn0_Forced_Output_Stop_Function1_Stop R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Stop R_KB2m_TKBOn0_DitheringFunction_Start R_KB2m_TKBOn0_DitheringFunction_Stop R_KB2m_TKBOn1_DitheringFunction_Start R_KB2m_TKBOn1_DitheringFunction_Stop R_KB2m_TKBOn0_SmoothStartFunction_Start R_KB2m_TKBOn0_SmoothStartFunction_Stop R_KB2m_TKBOn1_SmoothStartFunction_Start | A A A M A A A A A A A A A A A A A A A A A | |
| r_cg_kb2_user.c | M A | ||
| r_cg_kb2.h | - | - | 
Table 2.4 Output File List (4/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_rtc.c | R_RTC_Set_CalendarCounterValue R_RTC_Get_CalendarCounterValue R_RTC_Set_ConstPeriodInterruptOn | A A A A M A A A A A A A A A A A A A A A A A A A A A A | |
| r_cg_rtc_user.c | M A A A A A A | ||
| r_cg_rtc.h | - | - | |
| r_cg_fmc.c | A A A M | ||
| r_cg_fmc_user.c | M A | ||
| r_cg_fmc.h | - | - | 
Table 2.5 Output File List (5/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_it.c | A A A M M | ||
| r_cg_it_user.c | M A | ||
| r_cg_it.h | - | - | |
| r_cg_it8bit.c | A A A M M | ||
| r_cg_it8bit_user.c | M A | ||
| r_cg_it8bit.h | - | - | |
| r_cg_timer.c | A A A M | ||
| r_cg_timer_user.c | M A | ||
| r_cg_timer.h | - | - | |
| r_cg_pclbuz.c | A A A M | ||
| r_cg_pclbuz_user.c | M | ||
| r_cg_gpt.h | - | - | |
| r_cg_wdt.c | A A | ||
| r_cg_wdt_user.c | M A | ||
| r_cg_wdt.h | - | - | |
| r_cg_pga_dsad.c | A A A M A A A | ||
| r_cg_pga_dsad_user.c | r_pga_dsad_interrupt_conversion | M A A A A | |
| r_cg_pga_dsad.h | - | - | 
Table 2.6 Output File List (6/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_adc.c | A A A A A M M M M M M A A | ||
| r_cg_adc_user.c | M A | ||
| r_cg_adc.h | - | - | |
| r_cg_camp.c | A A A M | ||
| r_cg_camp_user.c | M | ||
| r_cg_camp.h | - | - | |
| r_cg_tmps.c | A A A M M | ||
| r_cg_tmps_user.c | M | ||
| r_cg_tmps.h | - | - | |
| r_cg_dsadci.c | A A A A A M M A A | ||
| r_cg_dsadc_user.c | M A A | ||
| r_cg_dsadc.h | - | - | 
Table 2.7 Output File List (7/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_dac.c | A A A M A A A A M | |||
| r_cg_dac_user.c | M M | |||
| r_cg_dac.h | - | - | ||
| r_cg_pga.c | A A A M M | |||
| r_pga_user.c | M | |||
| r_pga.h | - | - | ||
| r_cg_comp.c | A A A M M | |||
| r_cg_comp_user.c | M A | |||
| r_cg_comp.h | - | - | ||
| r_cg_comppgacmpb.c | A M A A A A A A | |||
| r_cg_comppga_user.c | M A | |||
| r_cg_comppga.h | - | - | ||
Table 2.8 Output File List (8/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_serial.c or r_cg_sau.c | A M M M M A A A A A A A A A A A A A A A A A | |||
| r_cg_serial_user.c or r_cg_sau_user.c | r_uartn_callback_softwareoverrun r_iicmn_callback_master_sendend | M A A A A A A A A A A A A A A A | ||
| r_cg_serial.h or r_cg_sau.h | - | - | ||
| r_cg_serial.c | A A A A A | |||
| r_cg_serial_user.c | A A A A A A A | |||
| r_cg_serial.h | - | - | ||
Table 2.9 Output File List (9/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | 
| r_cg_serial.c | A A A M A A A A | ||
| r_cg_serial_user.c | r_uartfn_callback_softwareoverrun | M A A A A A A A A A | |
| r_cg_serial.h | - | - | |
| r_cg_serial.c or r_cg_iica.c | A M A M M A A A A A A A A | ||
| r_cg_serila_user.c or r_cg_iica_user.c | r_iican_callback_master_sendend r_iican_callback_master_receiveend r_iican_callback_slave_sendend | M A A A A A A A M | |
| r_cg_serial.h or r_cg_iica.h | - | - | |
| r_cg_lcd.c | A A A A A A A A | ||
| r_cg_lcd_user.c | M A | ||
| r_cg_lcd.h | - | - | 
Table 2.10 Output File List (10/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_sg.c | A A A | |||
| r_cg_sg_user.c | M A | |||
| r_cg_sg.h | - | - | ||
| r_cg_dmac.c | A A A A A | |||
| r_cg_dmac_user.c | M M A | |||
| r_cg_dmac.h | - | - | ||
| r_cg_dtc.c | A A A M A A | |||
| r_cg_dtc_user.c | M | |||
| r_cg_dtc.h | - | - | ||
| r_cg_elc.c | A A | |||
| r_cg_elc_user.c | M | |||
| r_cg_elc.h | - | - | ||
| r_cg_intc.c | A A A A A A A A A A | |||
| r_cg_intc_user.c | M A A A A | |||
| r_cg_intc.h | - | - | ||
Table 2.11 Output File List (11/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_intc.c or r_cg_key.c | A A A | |||
| r_cg_key_user.c | M A | |||
| r_cg_opamp.h | - | - | ||
| r_cg_doc.c | A A A A A A A A A A A A | |||
| r_cg_doc_user.c | M A A A A A M A | |||
| r_cg_doc.h | - | - | ||
| r_cg_bup.c | A A A | |||
| r_cg_bupt_user.c | M A | |||
| r_cg_bupt.h | - | - | ||
| r_cg_osdc.c | A A A M M | |||
| r_cg_osdc_user.c | M A | |||
| r_cg_osdc.h | - | - | ||
| r_cg_saic.c or r_cg_spi.c | A A M A A A | |||
| r_cg_saic_user.c or r_cg_spi_user.c | M M | |||
| r_cg_saic.h or r_cg_spi.h | - | - | ||
Table 2.12 Output File List (12/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_opamp.c | R_OPAMP_Set_ReferenceCircuitOn | A A A A A M M | ||
| r_cg_opamp_user.c | M | |||
| r_cg_opamp.h | - | - | ||
| r_cg_doc.c | A A A A A M M | |||
| r_cg_doc_user.c | M A | |||
| r_cg_doc.h | - | - | ||
| r_cg_mac32bit.c | A M M M M M M | |||
| r_cg_mac32bit_user.c | M A | |||
| r_cg_mac32bit.h | - | - | ||
| r_cg_12adc.c | R_12ADC_TemperatureSensorOutput_On R_12ADC_TemperatureSensorOutput_Off R_12ADC_InternalReferenceVoltage_On | A A A A M M M M M M | ||
| r_cg_12adc_user.c | M A | |||
| r_cg_12adc.h | - | - | ||
| r_cg_12da.c | A A A M A | |||
| r_cg_12adc_user.c | M | |||
| r_cg_12adc.h | - | - | ||
Table 2.13 Output File List (13/13)
| Peripheral Function | File Name | API Function Name | out put (*1) | |
| r_cg_ampansw.c | R_OPAMPm_Set_ReferenceCircuitOn | A A A A A A A | ||
| r_cg_ampansw_user.c | M | |||
| r_cg_ampansw.h | - | - | ||
| r_cg_vr.c | A A A | |||
| r_cg_vr_user.c | M | |||
| r_cg_vr.h | - | - | ||
*1 In case of [API output control] setting are default ([Output all API functions according to the setting]).
A:Output by settings on each peripheral functions panel automatically.
M:Output by the file used setting in API property.