r_atuiv_timerknm_comparex_interrupt
|
Performs processing in response to the compare match compare register and counter interrupt
[Syntax]
void r_atuiv_timerknm_comparex_interrupt ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number, x is the register number. |
[Argument(s)]
None.
[Return value]
None.