R_ATUIV_Timerknm_xpin_Output_Low
|
Output of pin provides low output.
[Syntax]
void R_ATUIV_Timerknm_xpin_Output_Low ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number, x is the output pin. |
[Argument(s)]
None.
[Return value]
None.