r_atuiv_timerknm_interrupt
|
Performs processing in response to the timer interrupt (Input capture, compare match).
[Syntax]
void r_atuiv_timerknm_interrupt ( void );
|
void r_atuiv_timerkn_channelm_interrupt ( void );
|
Remark | k is the timer kind, n is the unit number, m is the channel number. |
[Argument(s)]
None.
[Return value]
None.