Everything

R_ATUIV_Timerkn_Create_UserInit


Performs user-defined initialization relating to the each timer functions.

Remark

This API functions is called as the R_ATUIV_Timerkn_Create callback routine.

[Syntax]

void    R_ATUIV_Timerk_Create_UserInit ( void );
void    R_ATUIV_Timerkn_Create_UserInit ( void );

Remark

k is the timer kind, n is the unit number.

[Argument(s)]

None.

[Return value]

None.