R_ATUIV_Timerknm_Set_Compare_Match
Sets the compare match register.
[Syntax]
void R_ATUIV_Timerknm_Set_Compare_Match ( void );
Remark
k is the timer kind, n is the unit number, m is the channel number.
[Argument(s)]
None.
[Return value]