R_ATUIV_Timerknm_Start_Down_Count
Starts the down count.
[Syntax]
void R_ATUIV_Timerknm_Start_Down_Count ( void );
Remark
k is the timer kind, n is the unit number, m is the channel number.
[Argument(s)]
None.
[Return value]