R_ATUIV_Timerkn_Create
Performs initialization necessary to control the each timer functions.
[Syntax]
void R_ATUIV_Timerk_Create ( void );
void R_ATUIV_Timerkn_Create ( void );
Remark
k is the timer kind, n is the unit number.
[Argument(s)]
None.
[Return value]