This function sets performance measurement. [RH850][E1/E2/E20/Full-spec emulator/IE850A]
Specify a condition of performance measurement. See the PerformanceCondition class for a condition of performance measurement. |
If performance measurement was set successfully: Performance measurement event number
If there was an error when setting performance measurement: None
This function sets performance measurement according to the contents specified with PerformanceCondition. |