Everything

debugger.Trace.Delete


This function deletes a conditional trace.

[Specification format]

debugger.Trace.Delete(timerNumber = "")

[Argument(s)]

Argument

Description

timerNumber

Specify the trace event number to delete.

[Return value]

If a trace was deleted successfully: True

If there was an error when deleting a trace: False

[Detailed description]

-

This function deletes the trace of the trace event number specified by tracenumber.

-

If traceNumber is not specified, then traces of all trace event numbers will be deleted.

[Example of use]

>>>debugger.Trace.Delete(1)
True
>>>