Everything

debugger.Breakpoint.Delete


This function deletes a break point.

[Specification format]

debugger.Breakpoint.Delete(breakNumber = "")

[Argument(s)]

Argument

Description

breakNumber

Specify the break event number to delete.

[Return value]

If a break point was deleted successfully: True

If there was an error when deleting a break point: False

[Detailed description]

-

This function deletes the break event specified by breakNumber.

-

If breakNumber is not specified, then breaks of all break event numbers will be deleted.

[Example of use]

>>>debugger.Breakpoint.Enable(1)
True
>>>debugger.Breakpoint.Disable(1)
True
>>>debugger.Breakpoint.Delete(1)
True
>>>