debugger.Interrupt.RequestFE
|
This function sends an FE-level interrupt request to the interrupt controller. [RH850 Simulator (G4MH)]
[Specification format]
debugger.Interrupt.RequestFE(channelNumber)
|
[Argument(s)]
|
|
channelNumber
|
Specify the channel number of the FE-level interrupt.
|
[Return value]
If the interrupt request was successful :True
If the interrupt request failed :False
[Detailed description]
- | This function sends an FE-level interrupt request to the interrupt controller. |
- | Generation of the interrupt depends on the settings and state of the interrupt controller. |
[Example of use]
>>>debugger.Interrupt.RequestFE(0)
True
>>>
|