debugger.Memory.ReadRange
|
This function refers to the specified number of locations in memory.
[Specification format]
debugger.Memory.ReadRange(address, count, memoryOption = MemoryOption.Byte)
|
[Argument(s)]
|
|
address
|
Specify the start address to reference.
|
count
|
Specify the number of locations in memory for reference.
|
memoryOption
|
Specify the display unit.
The units that can be specified are shown below.
|
|
|
MemoryOption.Byte
|
Byte unit (8 bits) (default)
|
MemoryOption.HalfWord
|
Half-word unit (16 bits) [RH850,RX,V850]
|
MemoryOption.Word
|
Word unit (RL78,78K: 16 bits, RH850,RX,V850: 32 bits)
|
[Return value]
List of referenced memory value (numeric value)
[Detailed description]
- | This function displays, in hexadecimal notation, the number of values specified by count with the width in memory specified by memoryOption in the range from the address specified by address. |
- | In case of failure to acquire a value from memory, "?" is displayed (0x??, 0x????, and 0x???????? in the 8-, 16-, and 32-bit cases, respectively). |
[Example of use]
>>>debugger.Memory.ReadRange(0x100, 3, MemoryOption.Word)
0x00000011 0x0000ff30 0x0000ff40
>>>mem = debugger.Memory.ReadRange(0x1ffffd, 5, MemoryOption.Byte)
0x23 0x43 0x32 0x?? 0x??
>>>print mem[0]
35
|