Everything

debugger.ActionEvent.Delete


This function deletes an action event.

[Specification format]

debugger.ActionEvent.Delete(actionEventNumber = "")

[Argument(s)]

Argument

Description

actionEventNumber

Specify the action event number to delete.

[Return value]

If an action event was deleted successfully: True

If there was an error when deleting an action event: False

[Detailed description]

-

This function deletes the action event specified by actionEventNumber.

-

If actionEventNumber is not specified, then events of all action event numbers will be deleted.

[Example of use]

>>>debugger.ActionEvent.Delete(1)
True
>>>debugger.ActionEvent.Delete()
True
>>>