Everything

debugger.Interrupt.RequestFENMI


This function sends an NMI request to the interrupt controller. [RH850 Simulator (G4MH)]

[Specification format]

debugger.Interrupt.RequestFENMI()

[Argument(s)]

None

[Return value]

If the interrupt request was successful : True

If the interrupt request failed : False

[Detailed description]

-

This function sends an NMI request to the interrupt controller.

-

Generation of the interrupt depends on the settings and state of the interrupt controller.

[Example of use]

>>>debugger.Interrupt.RequestFENMI()
True
>>>