Everything

debugger.ActionEvent.Set


This function sets an action event.

[Specification format]

debugger.ActionEvent.Set(ActionEventCondition)

[Argument(s)]

Argument

Description

ActionEventCondition

Specify a condition of an action event.

See the ActionEventCondition class for creating an action event.

[Return value]

Set action event number (numerical value)

[Detailed description]

-

This function sets an action event according to the contents specified with ActionEventCondition.

-

The specified action event is registered with the following name.

Python Action Eventnumerical-value

[Example of use]

>>>ae = ActionEventCondition()
>>>ae.Address = "main"
>>>ae.Output = "chData = "
>>>ae.Expression = "chData"
>>>ae.ActionEventType = ActionEventType.Printf
>>>ae_number = debugger.ActionEvent.Set(ae)
1
>>>print ae_number
1