cvtf.uws


浮動小数点形式への変換(単精度)を行います。(Floating-point Convert Unsigned-Word to Single (Single))

[指定形式]

-

cvtf.uws reg1, reg2

[機能]

汎用レジスタreg1にある符号のない32ビットの整数形式の内容を算術的に単精度浮動小数点形式に変換し,汎用レジスタreg2に格納します。結果は,現在の丸めモードに従って丸めます。

[詳細説明]

-

アセンブラでは,機械語命令のcvtf.uws命令が1つ生成されます。