Everything
 

Combination Condition dialog box [E1][E20]


This dialog box is used to display and modify detailed information on the combination break event selected in the Events panel.

Figure A.35

Combination Condition Dialog Box

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to the combination break event [E1][E20], then select [Edit Condition...] from the context menu.

[Description of each area]

(1)

Tab selection area

In this product version, the [Break] tab is displayed in this area.

(2)

[Combination] area

Select the combination condition from the following drop-down list.

OR

The condition is satisfied when one of the events listed in the [Object event] area is encountered (default).

Sequential

The condition is satisfied when the events listed in the [Object event] area are encountered in the specified sequence.

Caution

When [OR] is selected, up to two break events can be specified.
When [Sequential] is selected, break event can be specified for the 1st to 2nd position.

(3)

[Object event] area

(a)

Display of the list

This area lists the detailed information on the object events to be combined.

When [Sequential] is specified in the [Combination] area, numbers are allocated to each item from the top of the list to indicate the order in which the conditions are to be satisfied.

(b)

Buttons

The following buttons are enabled only when [Sequential] is selected in the [Combination] area.

Button

Function

Up

Moves the event serial number upward in the target event list.

Down

Moves the event serial number downward in the target event list.

R Event

This button is always invalid.

(4)

[Reset event] area

(a)

Display of the list

This area is always invalid.

[Function buttons]

Button

Function

OK

Applies the detailed settings specified in the dialog box to the combination break and closes this dialog box.

Cancel

Cancels the save and closes this dialog box.

Help

Displays the help for this dialog box.