Everything
 

Memory Mapping dialog box


This dialog box is used to display the state of the memory mapping.

Figure A.20

Memory Mapping Dialog Box

 

This section describes the following.

[How to open]

-

On the [Debug Tool Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [Memory mappings] property in the [Memory] category.

Caution

This dialog box cannot be opened during execution of a program.

[Description of each area]

(1)

Added memory mapping specification area

This area is always invalid.

(2)

[Memory mapped list] area

(a)

List display

Information about the microcontroller's internal memory mapping is displayed.

This area cannot be edited.

Memory type

Displays the memory types.

Address range

Displays the address range as <Start address> - <End address>.
Display is fixed as "0x"-prefixed hexadecimal numbers.

Size

Displays size as a decimal number (unit: bytes/KbytesNote).

Access width

Displays the access width (unit: bits).

Note

Only in the case of multiple of 1024, displays in kilobyte units.

(b)

Button

Button

Function

Remove

This button is always invalid.

[Function buttons]

Button

Function

OK

Closes this dialog box.

Cancel

Closes this dialog box.

Help

Displays the help for this dialog box.