Everything
 

Current Consumption Measurement Condition Setting dialog box [E2]


This dialog box is used to set measurement conditions in the Measuring Current Consumption panel [E2][Simulator].

Figure A.49

Current Consumption Measurement Condition Setting Dialog Box

 

This section describes the following.

[How to open]

-

On the Measuring Current Consumption panel [E2][Simulator], click the button on the toolbar.

[Description of each area]

(1)

[Operation after record memory is full]

Select the operation of the debugger after the recording memory of the emulator becomes full during the measurement of current consumption from the following drop-down list.

Overwrite to the record memory and continue execution

Continue to execute the program and to record data by overwriting the data from the beginning of the recording memory.

Stop recording

Only stop writing to the recording memory but continue to execute the program.

Stop program

Stop both writing to the recording memory and execution of the program.

(2)

[Sampling time]

Select the sampling time during the measurement of current consumption.

The following sampling times can be selected.

1us, 2us, 5us, 10us, 20us, 50us, 100us, 200us, 500us, 1ms

(3)

[Acquisition condition] area

Make settings regarding conditions for writing to the recording memory of the emulator.

(a)

[Condition]

Select the type of condition for writing to the recording memory of the emulator from the following drop-down list.

All

Record all measured data without restrictions.

During detecting an external trigger input

Record the measured data with use of the function for detecting an external trigger input in the extended interface of the E2 emulator only while the external trigger input is detected.

During monitor points

Record the measured data only over the time from detection of the monitoring point for starting measurement until detection of the monitoring point for ending measurement.

(b)

[Channel]

When "During detecting an external trigger input" is selected for [Condition], select "ch0" or "ch1" as the external trigger input channel from the extended interface of the E2 emulator that is to be detected.

(c)

[External trigger input type]

When "During detecting an external trigger input" is selected for [Condition], select "High" or "Low" as the level of the external trigger input signal to be detected.

(d)

[Monitor points range]

When "During monitor points" is selected for [Condition], select the two target monitoring points.

Monitoring points that have currently been specified for the project are displayed in a drop-down list.

The measured data will only be recorded from the time the monitoring point set in the left side has been detected until detection of the monitoring point set on the right side.

[Function buttons]

Button

Function

OK

Reflects the settings of the measurement conditions that were made in this dialog box to the Measuring Current Consumption panel [E2][Simulator].

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.