Everything
 

CPU Register panel


This panel is used to display the contents of the CPU register (general-purpose registers and control registers) and change the CPU register values (see "2.10.2 Display/change the CPU register").

This panel appears only when connected to the debug tool.

Remark 1.

This panel can be zoomed in and out by in the tool bar, or by moving the mouse wheel forward or backward while holding down the [Ctrl] key.

Remark 2.

When the separator line of each area in this panel is double-clicked, the width of the area changes to the shortest possible size that can display the contents of the area.

Figure A.11

CPU Register Panel

 

This section describes the following.

[How to open]

-

From the [View] menu, select [CPU Register].

[Description of each area]

(1)

[Register Name] area

The types of register are classified as categories (folders), and a list of the respective register names is displayed. Note that neither category names nor register names can be edited and deleted.

The meanings of the icons are as follows:

 

Indicates that the register name belonging to this category is displayed. When you double-click on the icon, or click on the "-" mark, the category is closed and the register name is hidden.

 

Indicates that the register name belonging to this category is hidden. When you double-click on the icon, or click on the "+" mark, the category is opened and the register name is displayed.

 

Indicates the name of the register. When you double-click on the icon, or click on the "+" or "-" marks, the name of the register part is displayed or hidden.

 

Indicates the name of the register part.

 

Category names and register names displayed are as follows (number of "+" marks before register names indicates the depth of the display level):

Table A.3

Category Names and Register Names in CPU Register Panel

Category Name

Register Name (Alias)

Bit Width

Description

General-purpose register

+ AX(RP0)

16

General-purpose register (current register bank)

++ X(R0)

8

++ A(R1)

8

+ BC(RP1)

16

++ C(R2)

8

++ B(R3)

8

+ DE(RP2)

16

++ E(R4)

8

++ D(R5)

8

+ HL(RP3)

16

++ L(R6)

8

++ H(R7)

8

Control register

+ PC

20

Program counter

+ PSW

8

Program status word

++ IE

1

Interrupt enable flag

++ Z

1

Zero flag

++ RBS1

1

Register bank selection flag

++ AC

1

Auxiliary carry flag

++ RBS0

1

Register bank selection flag

++ ISP1

1

In service priority flag

++ ISP0

1

In service priority flag

++ CY

1

Carry flag

+ SP

16

Stack pointer

+ ES

8

ES register

+ CS

8

CS register

General-purpose register: Register bank nNote

+ AX(RP0): Register bank n

16

General-purpose register (Register bank n)

+ X(R0): Register bank n

8

++ A(R1): Register bank n

8

+ BC(RP1): Register bank n

16

++ C(R2): Register bank n

8

++ B(R3): Register bank n

8

+ DE(RP2): Register bank n

16

++ E(R4): Register bank n

8

++ D(R5): Register bank n

8

+ HL(RP3): Register bank n

16

++ L(R6): Register bank n

8

++ H(R7): Register bank n

8

Note

"n" indicates the number of the register bank (n = 0, 1, 2, 3).

Table A.4

Category Names and Register Names in FAA Register Panel

Category Name

Register Name (Alias)

Bit Width

Description

Operation parameter register set

A0

32

Accumulator

M0

32

Multiplier register

M1

32

Shift count register

L0

32

Upper limit register

L1

32

Lower limit register

R0

32

Addend register

Address pointer set

DP0

12

Address pointer for accumulator

DP1

12

Address pointer for operation parameters

RP0

12

Address pointer for storing operation results

PG0

12

Program pointer

SP0

12

Stack pointer

Control Register

+FAACNT

16

Processor Control Register

++START

1

Program execution bit

+FAAFLG

16

Flag Bit Register

++I

1

Interrupt flag

++ZERO

1

Zero flag

++UNDER

1

Under flag

++OVER

1

Over flag

+SYSC

16

System Control Register

++EXE

1

Processor operating bit

++ENB

1

Operation enable bit

++SRST

1

Software reset bit

++SLP

1

Sleep bit

This area is provided with the following functions.

(a)

Registering watch-expression

CPU registers/categories can be registered in the Watch panel as watch-expressions.

See "2.10.6.1 Register a watch-expression" for details on how to operate it.

Remark 1.

When you have registered a watch-expression with a category as the object, all of the CPU registers belonging to that category are registered as watch-expressions.

Remark 2.

A scope specification is automatically added to a registered watch-expression.

(2)

[Value] area

The values of each CPU register are displayed and changed.

The radix of a data value can be selected by the button on the toolbar or the context menu item. In addition, a display format adding the value in hexadecimal number constantly can also be selected as well.

The meanings of the colors of the CPU register values are as follows (character colors and background colors depend on the configuration in the [General - Font and Color] category of the Option dialog box):

Display Example (Default)

Description

 

Character color

Blue

The value of the CPU register that the user is changing

Press the [Enter] key to write to the target memory.

Background color

Standard color

 

Character color

Brown

The value of the CPU register that has been changed because of the execution of a program.

The highlighting is rest by executing again the program.

Background color

Cream

 

This area is provided with the following functions.

(a)

Changing the CPU register value

To edit the CPU register value, select the value to edit, then change the value directly from the keyboard after clicking again on it (press the [Esc] key to cancel the edit mode).

After you edit the value of the CPU register, it is written to the target memory of the debug tool by pressing the [Enter] key or moving the focus to outside the edit region.

(b)

Saving the contents of the CPU register

The Save As dialog box can be opened by selecting the [File] menu >> [Save CPU Register Data As…], and all the contents of this panel can be saved in a text file (*.txt) or CSV file (*.csv).

See "2.10.2.4 Save the CPU register contents" for details on the method for saving the contents of the CPU register.

[Toolbar]

 

Acquires the latest data from the debug tool, and updates the contents of this panel.

This item is disabled during execution of a program.

Notation

The following buttons to change the notation of a data value are displayed.

 

AutoSelect

Displays the value of the selected item (including sub-items) in the default notation (default).

Hexadecimal

Displays the value of the selected item (including sub-items) in hexadecimal number.

Signed Decimal

Displays the value of the selected item (including sub-items) in signed decimal number.

Unsigned Decimal

Displays the value of the selected item (including sub-items) in unsigned decimal number.

Octal

Displays the value of the selected item (including sub-items) in octal number.

Binary

Displays the value of the selected item (including sub-items) in binary number.

ASCII

Displays the character string of the selected item (including sub-items) in ASCII code. If the character size is 2 bytes and above, it is displayed with the characters for each 1 byte arranged side-by-side.

Float

Displays the value of the selected item in Float.

Note that when the value is not 4-byte data, displays it in the default notation.

Double

Displays the value of the selected item in Double.

Note that when the value is not 8-byte data, displays it in the default notation.

 

Adds the value in hexadecimal number enclosing with "()" at the end of the value.

[[File] menu (CPU Register panel-dedicated items)]

The following items are exclusive for the [File] menu in the CPU Register panel (other items are common to all the panels).

Note that all these items are disabled during execution of a program.

Save CPU Register Data

Overwrites the contents of this panel to the previously saved text file (*.txt)/CSV file (*.csv) (see "(b) Saving the contents of the CPU register").

Note that when the file has never been saved or the file is write disabled, the same operation is applied as the selection in [Save CPU Register Data As…].

Save CPU Register Data As…

Opens the Save As dialog box to newly save the contents of this panel to the specified text file (*.txt)/CSV file (*.csv) (see "(b) Saving the contents of the CPU register").

[[Edit] menu (CPU Register panel-dedicated items)]

The following items are exclusive for [Edit] menu in the CPU Register panel (all other items are disabled).

Cut

Deletes the selected character string and copies it to the clipboard.

This item becomes valid only when the character string is being edited.

Copy

Copies the selected character string to the clipboard during editing.

If a line is selected, copies the register or the category to the clipboard.

The copied item can be pasted to the Watch panel.

Paste

Pasts the character string copied in the clipboard to the caret position.

This item becomes valid only when the character string is being edited.

Select All

Selects all the items of this panel.

Find…

Opens the Find and Replace dialog box with selecting the [Find in Files] tab.

Replace…

Opens the Find and Replace dialog box with selecting the [Replace in Files] tab.

[Context menu]

Register to Watch1

Registers the selected register or category to the Watch panel (Watch1).

Copy

Copies the selected character string to the clipboard during editing.

If a line is selected, copies the register or the category to the clipboard.

The copied item can be pasted to the Watch panel.

Notation

The following cascade menus to specify the notation of a data value are displayed.

 

AutoSelect

Displays the value of the selected item (including sub-items) in the default notation (default).

Hexadecimal

Displays the value of the selected item (including sub-items) in hexadecimal number.

Signed Decimal

Displays the value of the selected item (including sub-items) in signed decimal number.

Unsigned Decimal

Displays the value of the selected item (including sub-items) in unsigned decimal number.

Octal

Displays the value of the selected item (including sub-items) in octal number.

Binary

Displays the value of the selected item (including sub-items) in binary number.

ASCII

Displays the character string of the selected item (including sub-items) in ASCII code.

If the character size is 2 bytes and above, it is displayed with the characters for each 1 byte arranged side-by-side.

Float

Displays the value of the selected item in Float.

Note that when the value is not 4-byte data, displays it in the default notation.

Double

Displays the value of the selected item in Double.

Note that when the value is not 8-byte data, displays it in the default notation.

Include Hexadecimal Value

Adds the value in hexadecimal number enclosing with "()" at the end of the value.