Below is a list of API functions output by the Code Generator for clock serial interface G use.
Table 3.7
API Functions: [Clock serial interface G]
API Function Name
Function
R_CSIGm_Create
Performs initialization necessary to control the clock serial interface G functions.
R_CSIGm_Create_UserInit
Performs user-defined initialization relating to the clock serial interface G functions.
r_csigm_interrupt_receive
Performs processing in response to the CSIG reception interrupt.
r_csigm_interrupt_error
Performs processing in response to the CSIG error interrupt.
r_csigm_interrupt_send
Performs processing in response to the CSIG communication interrupt.
r_csigm_callback_receiveend
r_csigm_callback_sendend
r_csigm_callback_error
R_CSIGm_Start
Sets CSIG communication to standby mode.
R_CSIGm_Stop
Ends CSIG communication.
R_CSIGm_Send
Start CSIG data transmission.
R_CSIGm_Receive
Start CSIG data reception.