Below is a list of API functions output by the Code Generator for timer option use.
Table 3.17
API Functions: [Timer option]
API Function Name
Function
R_TAPAm_Create
Performs initialization necessary to control the timer option functions.
R_TAPAm_Create_UserInit
Performs user-defined initialization relating to the timer option functions.
R_TAPAm_Start
Enables asynchronous Hi-Z control.
R_TAPAm_Stop
Disables asynchronous Hi-Z control.
R_TAPAm_Trigger_Start
Sets the Hi-Z control signal to the low level.
R_TAPAm_Trigger_Stop
Sets the Hi-Z control signal to the high level.