Below is a list of API functions output by the Code Generator for port functions use.
Table 3.3
API Functions: [Port functions]
API Function Name
Function
R_PORT_Create
Performs initialization necessary to control the port functions.
R_PORT_Create_UserInit
Performs user-defined initialization relating to the port functions.